CRC for LVDS display of imx8qxp processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CRC for LVDS display of imx8qxp processor

1,676 Views
Ashil
Contributor I

We were interested in incorporating CRC or checksum functionality to perform integrity checks on specific zones or portions of soft tell-tale indicators displayed on our system. These checks are essential for ensuring the accuracy and reliability of critical information presented to our users.Can you command about this possibility for imx8qxp. Are there any recommended software libraries or functions for calculating CRC or checksums that are well-suited for the i.MX 8 platform

0 Kudos
Reply
3 Replies

1,612 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hi @Ashil,
 
I hope you are doing well.
 
Display Content Integrity Checker using CRC is supported in i.MX 8QuadXPlus Processors.
 
Please refer to 8.2 Display Content Integrity Checker (DCIC) and 8.2.7 DCIC CRC Calculation Functions in i.MX Linux Reference Manual for more information and functions for calculating CRC.
 
One can look at /test/mxc_dcic_test for the sample program.
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply

1,549 Views
Ashil
Contributor I

Hi,

Thanks for letting me know the example.

is this test/mxc_dcic_test/mxc_dcic_test.c source code checking the a frame from frame buffer.

In that case I had a question are we checking CRC of the frame which is comming as output of Display controller. or are we checking CRC of the frame which is input to the display controller

0 Kudos
Reply

1,506 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Ashil,

 
I hope you are doing well.
 

 

DCIC checks the CRC of the frame which is coming as the output of the Display controller.
 
DCIC driver is used for i.MX6Q series. i.MX8QXP uses dpu-crc module.
 
Please refer to the community post below for more information.

 

 
Thanks & Regards,

Sanket Parekh

0 Kudos
Reply