Hello all,
I am facing issue with linux-imx 3.14.28 kernel. I have a imx6solo sabre auto based board.
When I flash the kernel generated from Yocto (meta-fsl-arm), it gives the following error
-----------------------------------------------------------------------------------------------------------------------------------------
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xa0800000 - 0xff000000 (1512 MB)
lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x806d54ac (6966 kB)
.init : 0x806d6000 - 0x80a6a100 (3665 kB)
.data : 0x80a6c000 - 0x80aaa1e0 ( 249 kB)
.bss : 0x80aaa1ec - 0x80b0cc20 ( 395 kB)
*SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1*
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 512 kB
failed to set parent of clk gpu2d_core_sel to pll2_pfd1_594m: -22
Switching to timer-based delay loop
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every
1431655765682ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped) preset value.. 1581.05 BogoMIPS
(lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10516040 - 0x10516098
*CPU1: failed to boot: -38*
Brought up 1 CPUs
SMP: Total of 1 processors activated.
------------------------------------------------------------------------------------------------------------------------------------------
My board is solo, but the kernel debug messages show CPUs =2.
Also it gives error as CPU1:failed to boot. Do i need to change any
configurations in Yocto or kernel config to make CPUS=1?
-Thanks
Sharvari