COM Port is not Working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

COM Port is not Working

3,283 次查看
KrishnaPavan
Contributor II

COM Port is not working when I connect my board in this way

571-NOT_WORKED.png

 

I am using minicom, all the necessary drivers have been installed.

When I use Serial Cable I connect with minicom configured like this

573-serial_snap.pngWhen I use USB i use Serial Device as /dev/ttyUSB0 .

 

When I use a USB to Serial Connector, the board is then working fine, I mean I am able to communicate with my board.

 

The serial cable and COM Port if used individually are working fine.

Any idea about this problem?

 

Regards :: Krishna Pavan

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

3,086 次查看
KrishnaPavan
Contributor II

Hi,

As early mentioned I have been checking the DB9 connector.

 

Even the statserial software could show the same.

Which means that the COM Port is not receiving any data that is transmitted to it.

Here are the pics of the Stat Serial

I just connected the board, Now the booting sequence has been initiated after Power Up

575-statbeforestat.pngNow I need to enter the log-in that is by default root

Now that stats are577-statafter.png

Any Infererences?

Have any one faced the problem with the COM Ports on the board/PC.    Regards ::  Krishna Pavan

0 项奖励
回复

3,086 次查看
KrishnaPavan
Contributor II

The loop back test using gtkterm/minicom did not give me any result.

 

Is there an error within the board or is the error with my PC?

0 项奖励
回复

3,085 次查看
KrishnaPavan
Contributor II

The log is here

I am attaching a txt doc with the log pasted .

 

When I am supposed to type the freescale log-in I am not able to do so..

I am not able to type, which means that the transmission has got problem...

0 项奖励
回复