CCM_CLK1_P clock output 8MHz generating settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CCM_CLK1_P clock output 8MHz generating settings

1,034件の閲覧回数
prabhu1
Contributor III

Hi Igorpadykov,

Thanks for the reply, but I want to get the clock in CCM_CLK1_P pin expecting 8MHz clock (p17 pin i.mx6ull) what changes (any exact registers & dividers in inside processor) or from 24Mhz external clock source how to get 8Mhz clock inside processor? and connections between CCM_CLK1_P pin(p17) & 24Mhz clock inside IC ?

0 件の賞賛
返信
2 返答(返信)

954件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi prahbu

sorry this is not possible as answered on

CCM_CLK1_P clock output 8MHz generating settings 

Frequency options given in CCM_ANALOG_MISC1n[LVDS1_CLK_SEL] do not allow

such frequency.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

954件の閲覧回数
prabhu1
Contributor III

Hi Igorpadykov,

Then what frequencies can generate?

Please, could u give the steps, how to generate the clock on the CCM_CLK1_P pin(p17) and

what about CCM_CLK1_N pin(p16) leave float?

0 件の賞賛
返信