CAAM problem when boot for IMAX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAAM problem when boot for IMAX6Q

2,613件の閲覧回数
dengboping
Contributor I

In our  mass product, 3% are defective when boot, the log from serial port shows it shop at CAAM .

pastedImage_2.png

please give some help! Thanks

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,497件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   please refer to the following

https://community.nxp.com/message/850841 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,497件の閲覧回数
dengboping
Contributor I

Sorry, how to understand " The RNG Hardware error usually means that the entropy source has
failed to generate entropy
", what handware or software be related to it?

0 件の賞賛
返信

2,497件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   The following helps to clarify the issue with entropy 

Entropy and Random Number Generators @ Calomel.org 

Regards,

Yuri.

0 件の賞賛
返信

2,497件の閲覧回数
dengboping
Contributor I

It is random , 3  in 86 times  power on happened.

0 件の賞賛
返信