CAAM problem when boot for IMAX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAAM problem when boot for IMAX6Q

2,614 次查看
dengboping
Contributor I

In our  mass product, 3% are defective when boot, the log from serial port shows it shop at CAAM .

pastedImage_2.png

please give some help! Thanks

标签 (2)
0 项奖励
回复
4 回复数

2,498 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   please refer to the following

https://community.nxp.com/message/850841 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,498 次查看
dengboping
Contributor I

Sorry, how to understand " The RNG Hardware error usually means that the entropy source has
failed to generate entropy
", what handware or software be related to it?

0 项奖励
回复

2,498 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   The following helps to clarify the issue with entropy 

Entropy and Random Number Generators @ Calomel.org 

Regards,

Yuri.

0 项奖励
回复

2,498 次查看
dengboping
Contributor I

It is random , 3  in 86 times  power on happened.

0 项奖励
回复