CAAM features

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAAM features

Jump to solution
4,796 Views
fmajeric
Contributor III

Hi everyone,

I am studying the CAAM capabilities and performances on the iMX6 processor family. (In particular iMX6S, iMX6SX and iMX6Q).

Note that the CAAM runs in bare-metal applications (without any OS) on my boards.

  • I would like to know where is localized the CAAM in the SoC?
  • What is its clock /frequency ? Which PLL manages it ? Is the same clock for the CPU and the CAAM ?

        Is it possible to tune it ?

  • It is possible to get a performances benchmark of the differents crypto algorithms (AES, RSA, SHA...)
  • What is its hardware features ? Temperature, resistance ?

Untitled.png

I've already read

- i.MX 6Solo/6DualLite Applications Processor Reference Manual (IMX6SDLRM.pdf)

- i.MX 6 Series Thermal Management Guidelines (AN4579.pdf)

Is there others interestings documents ?

Anyone could give some informations ?

Thank you for your help,

Fabien M.

0 Kudos
Reply
1 Solution
4,067 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fabien

clocks used by caam are described in Table 18-3. System Clocks, Gating, and Override

i.MX6DQ Reference Manual (rev.2  7/2014)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Main info for caam  is security reference manual

https://community.freescale.com/docs/DOC-97660

Some performance link

https://community.freescale.com/docs/DOC-95700

Also it may be recommended to create service request (login to freescale.com)

for obtaining more performance data and localization in the SoC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
4,068 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fabien

clocks used by caam are described in Table 18-3. System Clocks, Gating, and Override

i.MX6DQ Reference Manual (rev.2  7/2014)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Main info for caam  is security reference manual

https://community.freescale.com/docs/DOC-97660

Some performance link

https://community.freescale.com/docs/DOC-95700

Also it may be recommended to create service request (login to freescale.com)

for obtaining more performance data and localization in the SoC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,067 Views
fmajeric
Contributor III

Hi,

thank you so much Igor. It's exactly what I'm looking for.

Best Regards,

Fabien.

0 Kudos
Reply