CAAM Test in imx6ulevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAAM Test in imx6ulevk

Jump to solution
2,755 Views
arunachalamrama
Contributor III

Hi

I am using imx6ulevk Yocto 4.1.15_2.0.0-ga.

How to verify CAAM is enabled?

I added imx-test to the image and could not find any test with caam name.

Please let me know which tests are available in imx-test for caam.

Regards,

Arun

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,112 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Configuration of CAAM driver is controlled by the kernel configuration parameters  under

Cryptographic API -> Hardware Crypto Devices.

  To call crypto algorithms from user space, the following kernel configuration parameters need

be selected  under Cryptographic API :

CRYPTO_USER_API_HASH

CRYPTO_USER_API_SKCIPHER

   Please refer to Chapter 50 CAAM (Cryptographic Acceleration and Assurance Module) in "i.MX_Linux_Reference_Manual.pdf" for detailed description about the configuration parameters.

  You can check the kernel boot log ; the following message is shown, if CAAM driver is loaded

successfully:

caam 2140000.caam: Instantiated RNG4 SH1

caam 2140000.caam: device ID = 0x0a16030000000000 (Era -524)

caam 2140000.caam: job rings = 3, qi = 0

caam algorithms registered in /proc/crypto

caam_jr 2141000.jr0: registering rng-caam

  To check algorithms registered, please use  /proc/crypto :

root@imx6ulevk:~# cat /proc/crypto

…

name              : cbc(aes)

driver              : cbc-aes-caam

module          : kernel

priority          : 3000

refcnt              : 1

selftest          : passed

internal          : no

type                : givcipher

async            : yes

blocksize      : 16

min keysize : 16

max keysize : 32

ivsize              : 16

geniv            : <built-in>

To check CAAM is working or not, you can run a simple test to do encryption operation,
using kernel crypto API, then check  /proc/interrupts.

root@imx6ulevk:~# cat /proc/interrupts

...

236:     14        GPC 105 Level     2141000.jr0

237:     0         GPC 106 Level    2142000.jr1

238:     0           GPC 46 Level       2143000.jr2

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

1 Reply
2,113 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Configuration of CAAM driver is controlled by the kernel configuration parameters  under

Cryptographic API -> Hardware Crypto Devices.

  To call crypto algorithms from user space, the following kernel configuration parameters need

be selected  under Cryptographic API :

CRYPTO_USER_API_HASH

CRYPTO_USER_API_SKCIPHER

   Please refer to Chapter 50 CAAM (Cryptographic Acceleration and Assurance Module) in "i.MX_Linux_Reference_Manual.pdf" for detailed description about the configuration parameters.

  You can check the kernel boot log ; the following message is shown, if CAAM driver is loaded

successfully:

caam 2140000.caam: Instantiated RNG4 SH1

caam 2140000.caam: device ID = 0x0a16030000000000 (Era -524)

caam 2140000.caam: job rings = 3, qi = 0

caam algorithms registered in /proc/crypto

caam_jr 2141000.jr0: registering rng-caam

  To check algorithms registered, please use  /proc/crypto :

root@imx6ulevk:~# cat /proc/crypto

…

name              : cbc(aes)

driver              : cbc-aes-caam

module          : kernel

priority          : 3000

refcnt              : 1

selftest          : passed

internal          : no

type                : givcipher

async            : yes

blocksize      : 16

min keysize : 16

max keysize : 32

ivsize              : 16

geniv            : <built-in>

To check CAAM is working or not, you can run a simple test to do encryption operation,
using kernel crypto API, then check  /proc/interrupts.

root@imx6ulevk:~# cat /proc/interrupts

...

236:     14        GPC 105 Level     2141000.jr0

237:     0         GPC 106 Level    2142000.jr1

238:     0           GPC 46 Level       2143000.jr2

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!