CAAM HASH algorithm performance Question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAAM HASH algorithm performance Question

4,869 次查看
zhongyue_li
Contributor II

Dear NXP engineers:

G'Day.

I am working on caam hash performance test on i.MX8 board.

and there is weird result that sha1 performance is lower than sha256's.

As far as i know, the computation of sha256 algorithm is more complicated that sha1's,

so i want to know why sha1 hash time is longer than sha256's.

I know the hash time is depend on the algorithm implementation.

Following is the test result, please help to confirm if it is normal data of test result?

Hash SHA1: 16 Mega byte data takes 94 milliseconds.

----------------------------------------------------

Job ring parameters:

g_job->dsc[0]:b0800007
g_job->dsc[1]:8441000d
g_job->dsc[2]:24540000
g_job->dsc[3]:84ef0a40
g_job->dsc[4]:1000000
g_job->dsc[5]:54200014
g_job->dsc[6]:81edef00

-----------------------------------------------------

Hash SHA256: 16 Mega byte data takes 81 milliseconds.

------------------------------------------------------

Job ring parameters:

g_job->dsc[0]:b0800007
g_job->dsc[1]:8443000d
g_job->dsc[2]:24540000
g_job->dsc[3]:84ef0a40
g_job->dsc[4]:1000000
g_job->dsc[5]:54200020
g_job->dsc[6]:81edef00

-----------------------------------------------------

Looking forward to you reply.

Thanks a bunch.

8 回复数

4,516 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  What i.MX8 device / board is used in the case? 

Regards,

Yuri.

0 项奖励
回复

4,516 次查看
zhongyue_li
Contributor II

Hello, Yuri,

I test these cases on i.mx8qxp b0 board with android os.

I use jobring3 in Trustzone to invoke CAAM hash function. 

Could you help check my test result?

Thanks a million.

0 项奖励
回复

4,516 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   which TEE they used to test SHA performance? OP-TEE or Trusty OS?

Regards,

Yuri.

0 项奖励
回复

4,516 次查看
zhongyue_li
Contributor II

Hello Yuri,

I test the case with Trusty OS.

Thank you.

0 项奖励
回复

4,516 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   preliminary considerations - it is possible to get SHA256 is faster than SHA1 when using CAAM,

depending on the optimization method of the SHA algorithms.

Regards,

Yuri.

0 项奖励
回复

4,516 次查看
zhongyue_li
Contributor II

Thanks for checking it,

so when can i get a exact point that SHA256 is faster than SHA1 when using CAAM?

Have a nice day.

0 项奖励
回复

4,516 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  app team  tried the SHA1 and SHA256 in Trusty OS with input data of 4k bytes.

It is shown that SHA256 is faster, than SHA1.  

  Note: It is recommended to use SHA256 -  as it is more secure than SHA1.

 

Regards,

Yuri.

0 项奖励
回复

4,516 次查看
zhongyue_li
Contributor II

Got it.

Thank you very much for helping check this issue.

I do appreciate it.

Best wishes.