CAAM API integration with U-Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAAM API integration with U-Boot

3,197 Views
kanimozhi_t
Contributor V

Hi,

    We would like to use CAAM for hash calculation and comparison on U-Boot. We know that we can use HAB APIs to utilise the CAAM internally but we're interested in using the CAAM directly for the above mentioned tasks.

    1. Is CAAM API available for public use? If so, where can we find the documentation?

    2. How can we integrate CAAM API on U-Boot? Are there any examples?

Any suggestions would highly be appreciated.

Labels (4)
Tags (3)
0 Kudos
Reply
3 Replies

3,179 Views
Yuri
NXP Employee
NXP Employee

@kanimozhi_t 
Hello,

  we do not support CAAM API for U-boot. Only Linux interface is available.

Regards,
Yuri.

3,174 Views
kanimozhi_t
Contributor V

Thank you @Yuri for the quick update.

 

BTW, can you share the links for CAAM Linux API?

3,164 Views
Yuri
NXP Employee
NXP Employee

@kanimozhi_t 
Hello,

    please refer to Chapter 8 (Security) of the NXP Linux RM.

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

 

Regards,
Yuri.