Bypass USB VBUS detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bypass USB VBUS detection

3,842件の閲覧回数
danielenderle
Contributor II

By design we cannot use OTG_VBUS Pin to detect if imx6 is connected as slave to a host machine. 

Is there a way to get USB OTG Slave mode working without using VBUS detection?

We are running Android 6.0.1/Linux 4.1.15.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,365件の閲覧回数
danielenderle
Contributor II

Hi Igor

i tried to find similiar source files where i can patch your suggested link but without any success.

Can you lead me to find the destination where i can patch those files for imx6?

Best regards

Daniel

0 件の賞賛
返信

3,365件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

may be helpful

I.MX6 : Using USB OTG without dynamic VBUS pin ? 

Best regards
igor

0 件の賞賛
返信

3,365件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

one can try to use similar patch for i.MX28

USB Device not work when VDD5V is not attached during boot (iMX28) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信