Burning an image to flexspi using MFG Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Burning an image to flexspi using MFG Tool

1,331 次查看
yanz
Contributor III

Hi all,

I'm trying to connect to flashloader using MFG Tool in order to burn an image into flexspi flash and get

yanz_0-1652783254686.png

What do I miss? The flexspi is enabled after rework and I'm able to communicate with.

Thank you in advance.

标签 (1)
0 项奖励
回复
3 回复数

1,310 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
According to the log, the BMOD[1:0] = 2'b10 (Internal Boot), I've no idea why you do that, it should set the BMOD[1:0] = '01' to enter the Serial Downloader mode.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,324 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I'd like to suggest you check the hardware connection such as the QSPI connection, next, you'd better confirm the Boot Device Configuration is match with hardware design.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,318 次查看
yanz
Contributor III

Thank you.

It's all about evk1050 after rework.

The SDK sample evkbimxrt1050_flash_component_nor works perfect.

SW7 set to

yanz_0-1652846392654.png

 

Nothing done except this.

Should it work? - SDCard, for example, flashed perfect when SW7 set to 

yanz_1-1652846497071.png

And below please find MFG tools log (thought that boot is from fuse):

-------MCU device Register----------
OCOTP->UUID[31:00] = 0x65f82484
OCOTP->UUID[63:32] = 0x3b1739d2
SRC->SBMR1 = 0x0
SRC->SBMR2 = 0x2000001
BMOD[1:0] = 2'b10 (Internal Boot)
HAB status = Open
--------MCU Flashloader info-------
Current Version = K2.1.0
Target Version = T1.0.0
--------MCU device eFusemap--------
(0x450) BOOT_CFG0 = 0x0
(0x460) BOOT_CFG1 = 0x0
(0x470) BOOT_CFG2 = 0x0
BT_FUSE_SEL = 1'b0
When BMOD[1:0] = 2'b00 (Boot From Fuses), It means there is no application in boot device, MCU will enter serial downloader mode directly
When BMOD[1:0] = 2'b10 (Internal Boot), It means MCU will boot application according to both BOOT_CFGx pins and Fuse BOOT_CFGx
----------FlexRAM memory-----------
IOMUXC_GPR->GPR16 = 0x200003
FlexRAM configuration is from eFuse
OCOTP->MISC_CONF0[31:00] = 0x40
FlexRAM Partion =0000 - 128KB ITCM, 128KB DTCM, 256KB OCRAM

Thank you in advance.

0 项奖励
回复