Burn OPT bits

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Burn OPT bits

跳至解决方案
2,508 次查看
garylijs
Contributor II

Hi ,

About the OTP bits setting, I have follow questions:

(1)If I can burn OTP bits from time to time in i.MX28?

(2)If freescale provide bit_settings.txt for i.MX28 secure boot, where I can get it?

Thanks very much.

标签 (1)
0 项奖励
回复
1 解答
2,347 次查看
igorpadykov
NXP Employee
NXP Employee

Hi gary

for secure boot please refer to AN4555 Secure Boot with i.MX28 HAB v4

utility for burning fuse:

IMX_OTP_TOOLS : A set of tools for managing OTP bits on the i.MX23 and i.MX28.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,347 次查看
garylijs
Contributor II

Btw, Our OS environment is Wince, not linux.

0 项奖励
回复
2,348 次查看
igorpadykov
NXP Employee
NXP Employee

Hi gary

for secure boot please refer to AN4555 Secure Boot with i.MX28 HAB v4

utility for burning fuse:

IMX_OTP_TOOLS : A set of tools for managing OTP bits on the i.MX23 and i.MX28.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复