Burn OPT bits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Burn OPT bits

Jump to solution
2,503 Views
garylijs
Contributor II

Hi ,

About the OTP bits setting, I have follow questions:

(1)If I can burn OTP bits from time to time in i.MX28?

(2)If freescale provide bit_settings.txt for i.MX28 secure boot, where I can get it?

Thanks very much.

Labels (1)
0 Kudos
Reply
1 Solution
2,342 Views
igorpadykov
NXP Employee
NXP Employee

Hi gary

for secure boot please refer to AN4555 Secure Boot with i.MX28 HAB v4

utility for burning fuse:

IMX_OTP_TOOLS : A set of tools for managing OTP bits on the i.MX23 and i.MX28.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,342 Views
garylijs
Contributor II

Btw, Our OS environment is Wince, not linux.

0 Kudos
Reply
2,343 Views
igorpadykov
NXP Employee
NXP Employee

Hi gary

for secure boot please refer to AN4555 Secure Boot with i.MX28 HAB v4

utility for burning fuse:

IMX_OTP_TOOLS : A set of tools for managing OTP bits on the i.MX23 and i.MX28.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply