Burn OPT bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,510件の閲覧回数
garylijs
Contributor II

Hi ,

About the OTP bits setting, I have follow questions:

(1)If I can burn OTP bits from time to time in i.MX28?

(2)If freescale provide bit_settings.txt for i.MX28 secure boot, where I can get it?

Thanks very much.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,349件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi gary

for secure boot please refer to AN4555 Secure Boot with i.MX28 HAB v4

utility for burning fuse:

IMX_OTP_TOOLS : A set of tools for managing OTP bits on the i.MX23 and i.MX28.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,349件の閲覧回数
garylijs
Contributor II

Btw, Our OS environment is Wince, not linux.

0 件の賞賛
返信
2,350件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi gary

for secure boot please refer to AN4555 Secure Boot with i.MX28 HAB v4

utility for burning fuse:

IMX_OTP_TOOLS : A set of tools for managing OTP bits on the i.MX23 and i.MX28.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信