Building standalone image for imx7dsabresd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Building standalone image for imx7dsabresd

1,472 次查看
econote_vikrant
Contributor III

Greetings!
I am trying to build linux image in standalone system for imx7dsabre board.
I am using TPS65185 PMIC, for which I have to patch some files in Kernel I built already, I have successfully patched files!
My questions are

1. How to build linux image for the same kernel through bitbake (kindly tell me exact process, I already read manual, the image I am building through bitbake as per the manual does not have drivers I patched up)

2. How to build root file system with the same kernel?

Kindly help as I am developing this image for epdc integration with i.MX7D SABRE

Thanks in advance!

标签 (4)
0 项奖励
回复
2 回复数

1,288 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vikrant 

may be useful to check

https://community.nxp.com/docs/DOC-1616 

i.MX Yocto Project: How can I (quickly) modify the kernel and test it? 

BSP porting guide: from a I.mx6q reference Board to a Custom board (in Yocto project) 

specific yocto questions also may be posted on meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,288 次查看
econote_vikrant
Contributor III

Thanks for your valuable reply, I will go through these all links and will update you on the same!

Regards,
Vikrant

0 项奖励
回复