Building i.MX6 Platform SDK in Windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building i.MX6 Platform SDK in Windows

5,321 Views
shamiksaha
Contributor II

Hi all,

I have a windows 32-bit pc. I have installed ARM DS-5 and arm-none-eabi toolchain and associated build tools in it.

Please guide me as to how to build the platform sdk to generate the binary file.

Thanks,

Shamik

0 Kudos
Reply
12 Replies

4,224 Views
Yuri
NXP Employee
NXP Employee

   The  SDK  is built  using  the  Mentor  Sourcery  CodeBench Lite  (previously  called  Sourcery  G++  Lite)

version  of  the  arm-­‐none-­‐eabi  GCC  toolchain. The  full  list  of  CodeBench  Lite releases  is  available  on  this  page:

< http://www.mentor.com/embedded-software/sourcery-tools/sourcery-codebench/editions/lite-edition/ >

It may be recommended to use Linux as host for SDK build, so please download Linux  installer  package. 
The  tarball packages  do  not  include  all executables.  Install  the  package  under  /opt  or  any other  local  folder, 

and  make  sure that  the  PATH environment  variable  allows accessing  these  executables  used  for  the build  process: 

CC = arm-none-eabi-gcc
CXX = arm-none-eabi-g++
AS = arm-none-eabi-as
AR = arm-none-eabi-ar
LN = arm-none-eabi-ld

Example  (sh syntax):

$ export PATH=$PATH:<toolchain_install_path>/bin


Source code installation

  The  SDK source  code  package  can  be  installed anywhere. It  is  not  recommended  to  use a  Windows  unzip  program 

to  extract the  sources,  as  this  may result  in line  endings  being  automatically  converted. Instead,  the  equivalent  command 

of  Linux should  be  used.

Example:

$ tar zxvf imx6_platform_sdk_v1.1.0.tgz


Build command

   To  build the  SDK,  use  the   ./tools/build_sdk  command.
Note:  It  is  important  to  run   build_sdk from  the  SDK  root  directory,  not  from within  the  tools directory.

Running make directly

If you want more control, you can run make directly:


$ make target=mx6dq board=smart_device  boardrev=a test=caam

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,224 Views
shamiksaha
Contributor II

Thanks for your reply Yuri, but I would like to know whether the SDK can be built using ARM DS-5 and what is the procedure to be followed.

Thanks,

Shamik

0 Kudos
Reply

4,224 Views
Yuri
NXP Employee
NXP Employee

  My experience is that Linux host and Codebench toolchain is the most easy way to

build the Platform SDK. Even under Cygwin I met issues, and we do not have experience

regarding the DS-5, sorry.

Regards,

Yuri.

0 Kudos
Reply

4,224 Views
nestle
Contributor III

For whatever reason, Mentor Graphics no longer lets us download Sourcery Codebench Lite.

They talk about it on their website but I cannot find any link in their Download section to get it.


Instead they want people to download Sourcery Codebench (commercial version) with a 30 day trail period.


So how the heck do I compile the SDK?  I don't want to install the 30 day trial edition.  I would like the lite edition.


Thanks

0 Kudos
Reply

4,224 Views
Yuri
NXP Employee
NXP Employee

I tried to build separate tests (succesfully): CAAM, PCIe, GPU, IPU.

Regards,

Yuri.

0 Kudos
Reply

4,224 Views
dhavalvadhar
Contributor IV

Hi Yuri,

How have you built those separate tests? Which toolchain have you used?

How can we get the same toolchain?

Please help us on this. I have been looking for resolution on this since long time, but still no luck.

Appreciate your prompt reply.

Thanks,

Dhaval

0 Kudos
Reply

4,224 Views
Yuri
NXP Employee
NXP Employee

Let me know Your e-mail.

Regards,

Yuri.

0 Kudos
Reply

4,224 Views
dhavalvadhar
Contributor IV

I may not be able to share my email id here on community.

0 Kudos
Reply

4,224 Views
Yuri
NXP Employee
NXP Employee

You may create SR via FSL Web.

Regards,

Yuri.

0 Kudos
Reply

4,224 Views
dhavalvadhar
Contributor IV

Hi Yuri,

Thanks for your quick response!

I have tried to share the email id using Private Message. But for that we should be connected i.e. you should be added as a friend. Can you please let me know how can I do that?

Thanks,

Dhaval

0 Kudos
Reply

4,224 Views
Yuri
NXP Employee
NXP Employee

It should be better just to create SR :

1.

Freescale Semiconductor | Embedded Processing Solutions

2.
Login (in order to get My Freescale Home page)


3.
Support


4.
Enter a Service Request to discuss confidential information

0 Kudos
Reply

4,224 Views
dhavalvadhar
Contributor IV

Hi Yuri,

Thanks for your help! I have generated the SR for the same.

BTW what is average TAT for SR?

Thanks,

Dhaval

0 Kudos
Reply