Building fsl-image-gui on Yocto dora

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building fsl-image-gui on Yocto dora

2,230 Views
dominicamann
Contributor III

I have followed the excellent tutorial by Daiane Angolini to download and build yocto. When building for imx6sabresd and building fsl-image-gui, the build stops with errors about include files in EGL (there were none).Has anyone else encountered this?

Labels (3)
5 Replies

1,651 Views
YixingKong
Senior Contributor IV

Dominic

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

1,651 Views
YixingKong
Senior Contributor IV

Dominic

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

1,651 Views
daiane_angolini
NXP Employee
NXP Employee

Could you, please, test it again today?

This issue was fixed during this weekend.

Oh, and thanks for the compliment ^.^


1,651 Views
LeonardoSandova
Specialist I

Which Linux flavor are you using to compile? Ubuntu 12.04 is perhaps the most tested host, at least for iMX

Leo

0 Kudos
Reply

1,651 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I followed the tutorial too, but I did not get any problem.

DaianeAngolini Do you have an idea of the possible problem?

Best Regards,

Alejandro

0 Kudos
Reply