Building Kernel Image Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building Kernel Image Issue

ソリューションへジャンプ
4,597件の閲覧回数
freewaymad
Contributor IV

Hi,

I am getting this error and I don't know why. I am following the "Android User's Guide" for building a kernel. Here is what I am getting:

now@Here:~$ export PATH=~/mydroid/jb/bootable/bootloader/uboot-imx/tools:$PATH

now@Here:~$ cd mydroid/jb/kernel_imx

now@Here:~/mydroid/jb/kernel_imx$ echo $ARCH && echo $CROSS_COMPILE

now@Here:~/mydroid/jb/kernel_imx$ export ARCH=arm

now@Here:~/mydroid/jb/kernel_imx$ export CROSS_COMPILE=~/myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-

now@Here:~/mydroid/jb/kernel_imx$ make imx6_android_defconfig

#

# configuration written to .config

#

now@Here:~/mydroid/jb/kernel_imx$ make uImage

make: /home/now/myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-gcc: Command not found

scripts/kconfig/conf --silentoldconfig Kconfig

make: /home/now/myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-gcc: Command not found

  CHK     include/linux/version.h

  CHK     include/generated/utsrelease.h

make[1]: `include/generated/mach-types.h' is up to date.

  CC      kernel/bounds.s

/bin/sh: 1: /home/now/myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-gcc: not found

make[1]: *** [kernel/bounds.s] Error 127

make: *** [prepare0] Error 2

now@Here:~/mydroid/jb/kernel_imx$

What am I doing wrong? Am I missing something? I am using Ubuntu 14.04 and the JB4.3_1.1.0 GA source. Please help.

Thank you,

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 解決策
2,407件の閲覧回数
freewaymad
Contributor IV

This case was that the path was not set correctly. Always double check the path.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,408件の閲覧回数
freewaymad
Contributor IV

This case was that the path was not set correctly. Always double check the path.

0 件の賞賛
返信
2,407件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

The Android project recommends using Ubuntu 12.04 64-bits, although only the 64 bits constraint is a must after Gingerbread.

Did you follow all the steps on the Android User’s Guide in order to install required packages and patches for our Android BSP? If so in which step are you finding this error? Sometimes it’s easy to overlook steps or packages like for example installing mkimage (command below)

$sudo apt-get install uboot-mkimage

That being said, it seems that the path to the toolchain is not being taken correctly. Please check this patch and make sure the files are there. If necessary, add to the .bashrc file.

0 件の賞賛
返信
2,407件の閲覧回数
freewaymad
Contributor IV

Hi,

Yes I have all the right packages. I'll check path to the toolchain.

Thanks,

0 件の賞賛
返信