Build linux kernel(3.14.28) for i.MX 6 without yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build linux kernel(3.14.28) for i.MX 6 without yocto

Jump to solution
6,018 Views
dhavalvadhar
Contributor IV

Hi,

I was able to build the images using Yocto build system. I have done that using command 'bitbake core-image-minimal'. Now during reading some document I found that the downloaded kernel source is available at location '<build dir>/tmp/work/imx6slevk-poky-linux-gnueabi/linux-imx/3.14.28-r0/git'. And I can compile it and boot the device using it.

To compile the kernel, I followed steps mentioned here. From this I am following steps for 'Building Kernel without BSP', without downloading the source from git. As the source is already available in the Yocto project. The Linux Kernel version is 3.14.28.

First I tried to build using 'make imx_v6_v7_defconfig' configuration. But for that I am getting following errors:

***************************************************************************************************************************

arch/arm/mach-imx/built-in.o: In function `clk_pllv3_do_shared_clks':

:(.text+0x1780): undefined reference to `imx_sema4_mutex_lock'

:(.text+0x17a8): undefined reference to `imx_sema4_mutex_unlock'

:(.text+0x17e0): undefined reference to `imx_update_shared_mem'

:(.text+0x17fc): undefined reference to `amp_power_mutex'

:(.text+0x1800): undefined reference to `shared_mem'

arch/arm/mach-imx/built-in.o: In function `clk_gate2_do_shared_clks':

:(.text+0x1a30): undefined reference to `imx_sema4_mutex_lock'

:(.text+0x1a58): undefined reference to `imx_sema4_mutex_unlock'

:(.text+0x1a98): undefined reference to `imx_update_shared_mem'

:(.text+0x1ab8): undefined reference to `amp_power_mutex'

:(.text+0x1abc): undefined reference to `shared_mem'

arch/arm/mach-imx/built-in.o: In function `clk_pfd_do_shared_clks':

:(.text+0x1e24): undefined reference to `imx_sema4_mutex_lock'

:(.text+0x1e4c): undefined reference to `imx_sema4_mutex_unlock'

:(.text+0x1e8c): undefined reference to `imx_update_shared_mem'

:(.text+0x1eac): undefined reference to `amp_power_mutex'

:(.text+0x1eb0): undefined reference to `shared_mem'

arch/arm/mach-imx/built-in.o: In function `imx6sl_set_wait_clk':

:(.text+0x61f8): undefined reference to `low_bus_freq_mode'

arch/arm/mach-imx/built-in.o: In function `imx6q_pm_enter':

:(.text+0x6d64): undefined reference to `imx_mu_enable_m4_irqs_in_gic'

:(.text+0x6de0): undefined reference to `imx_mu_is_m4_in_low_freq'

:(.text+0x6df4): undefined reference to `imx_mu_enable_m4_irqs_in_gic'

arch/arm/mach-imx/built-in.o: In function `imx6q_map_io':

:(.init.text+0xe7a4): undefined reference to `imx6_busfreq_map_io'

arch/arm/mach-imx/built-in.o: In function `imx6sl_map_io':

:(.init.text+0x115e0): undefined reference to `imx6_busfreq_map_io'

drivers/built-in.o: In function `fec_runtime_resume':

:(.text+0x119f00): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `fec_runtime_suspend':

:(.text+0x119f1c): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `imx_controller_resume':

:(.text+0x1666d4): undefined reference to `request_bus_freq'

:(.text+0x1666f4): undefined reference to `release_bus_freq'

:(.text+0x166788): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `imx_controller_suspend':

:(.text+0x16685c): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `ci_hdrc_imx_remove':

:(.text+0x166954): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `ci_hdrc_imx_probe':

:(.text+0x166d10): undefined reference to `request_bus_freq'

:(.text+0x166d30): undefined reference to `release_bus_freq'

:(.text+0x166e1c): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `sdhci_esdhc_runtime_resume':

:(.text+0x1c82d0): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `sdhci_esdhc_runtime_suspend':

:(.text+0x1c8344): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `sdhci_esdhc_imx_probe':

:(.text+0x1c8fdc): undefined reference to `release_bus_freq'

:(.text+0x1c9004): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `vpu_runtime_resume':

:(.text+0x1c949c): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `vpu_runtime_suspend':

:(.text+0x1c94b8): undefined reference to `release_bus_freq'

sound/built-in.o: In function `fsl_ssi_runtime_resume':

:(.text+0x2f160): undefined reference to `request_bus_freq'

sound/built-in.o: In function `fsl_ssi_runtime_suspend':

:(.text+0x2f17c): undefined reference to `release_bus_freq'

sound/built-in.o: In function `fsl_spdif_runtime_resume':

:(.text+0x30e08): undefined reference to `request_bus_freq'

sound/built-in.o: In function `fsl_spdif_runtime_suspend':

:(.text+0x30e24): undefined reference to `release_bus_freq'

make: *** [vmlinux] Error 1

***************************************************************************************************************************

After this I have tried with imx_v7_defconfig. And for this I am getting following errors:

***************************************************************************************************************************

drivers/usb/chipidea/ci_hdrc_imx.c: In function 'ci_hdrc_imx_notify_event':

drivers/usb/chipidea/ci_hdrc_imx.c:226:4: error: implicit declaration of function 'pinctrl_select_state' [-Werror=implicit-function-declaration]

    ret = pinctrl_select_state(data->pinctrl,

    ^

drivers/usb/chipidea/ci_hdrc_imx.c: In function 'ci_hdrc_imx_probe':

drivers/usb/chipidea/ci_hdrc_imx.c:278:2: error: implicit declaration of function 'devm_pinctrl_get' [-Werror=implicit-function-declaration]

  data->pinctrl = devm_pinctrl_get(&pdev->dev);

  ^

drivers/usb/chipidea/ci_hdrc_imx.c:278:16: warning: assignment makes pointer from integer without a cast

  data->pinctrl = devm_pinctrl_get(&pdev->dev);

                ^

drivers/usb/chipidea/ci_hdrc_imx.c:283:3: error: implicit declaration of function 'pinctrl_lookup_state' [-Werror=implicit-function-declaration]

   pinctrl_hsic_idle = pinctrl_lookup_state(data->pinctrl, "idle");

   ^

drivers/usb/chipidea/ci_hdrc_imx.c:283:21: warning: assignment makes pointer from integer without a cast

   pinctrl_hsic_idle = pinctrl_lookup_state(data->pinctrl, "idle");

                     ^

drivers/usb/chipidea/ci_hdrc_imx.c:299:29: warning: assignment makes pointer from integer without a cast

   data->pinctrl_hsic_active = pinctrl_lookup_state(data->pinctrl,

                             ^

cc1: some warnings being treated as errors

make[3]: *** [drivers/usb/chipidea/ci_hdrc_imx.o] Error 1

make[2]: *** [drivers/usb/chipidea] Error 2

make[1]: *** [drivers/usb] Error 2

make: *** [drivers] Error 2

***************************************************************************************************************************

I have exported all the necessary environment variables to build the kernel. At the moment I am using i.MX6 Sololite EVK.

Please guide me resolve these errors. Appreciate your quick help.

Thanks,

Dhaval

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,102 Views
dhavalvadhar
Contributor IV

Hello,

I have found the LOADADDR value for SLEVK and it should be 0x80008000. For other boards it can be found by considering 'UBOOT_ENTRYPOINT' variable from "<source directory>/meta-fsl-arm/conf/machine/include/imx-base.inc" file.

Hope this helps!

Thank you all for helping me!

Dhaval

View solution in original post

0 Kudos
Reply
6 Replies
3,102 Views
Yuri
NXP Employee
NXP Employee

  Please configure correctly Yocto environment, as described in 
section 5.2 (Machine configurations) of "Freescale_Yocto_Project_User's_Guide.pdf"

http://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,102 Views
dhavalvadhar
Contributor IV

Hi Yuri,

Thanks for your quick reply!

I have followed all the steps mentioned in the Yocto Project User's Guide.pdf. As I mentioned in my previous email I was able to build the *.sdcard image and able to boot the board using that image. Even using that filesystem and kernel I was able to boot the board using NFS.

After this I download the toolchain using 'bitbake meta-toolchain' and install it at default directory '/opt/poky/1.7' path. Using this toolchain I am able to build the sample driver module 'Hello World!' and able to run it on the board. Now I would like to build the kernel using the toolchain and where I am getting above mentioned errors.

Please help me to resolve the same. Appreciate your quick reply!

Thanks,

Dhaval

0 Kudos
Reply
3,102 Views
saurabh206
Senior Contributor III

Hi Dhaval

make  imx_v7_defconfig ARCH=arm CROSS_COMPILE=/opt/poky/1.5.1/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi- -j16 uImage LOADADDR=0x10008000

Correct your poky tool-chain path in above command.

0 Kudos
Reply
3,102 Views
dhavalvadhar
Contributor IV

Hi Saurabh,

Thanks for your quick reply!

The environment variables were set for ARCH and CROSS_COMPILE by command 'source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi'. And after that I ran 'make imx_v7_defconfig;make uImage' commands to build the kernel.

Thanks,

Dhaval

0 Kudos
Reply
3,102 Views
dhavalvadhar
Contributor IV

Hi Saurabh/Yuri,

Now I am able to build the kernel!! Though I don't know, how that happen. I haven't done anything special. Just freshly checkout the linux kernel using 'bitbake' command and try one more time today with same commands. But now I am getting errors for the load address. Can you please help me with that  for i.MX6 SLEVK?

BTW how one can decide the load address? I mean, what if I shift from SLEVK to some other board, how can I decide the load address.

Thanks,

Dhaval

0 Kudos
Reply
3,103 Views
dhavalvadhar
Contributor IV

Hello,

I have found the LOADADDR value for SLEVK and it should be 0x80008000. For other boards it can be found by considering 'UBOOT_ENTRYPOINT' variable from "<source directory>/meta-fsl-arm/conf/machine/include/imx-base.inc" file.

Hope this helps!

Thank you all for helping me!

Dhaval

0 Kudos
Reply