Build error in bitbake imx-image-multimedia for imx8mpevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build error in bitbake imx-image-multimedia for imx8mpevk

918 Views
ShivM
Contributor II

Hi,

I am trying to build imx-image-multimedia for imx8mpevk.

I have set MACHINE =  'imx8mpevk' DISTRO = 'fsl-imx-wayland' and below build config:

Build Configuration:
BB_VERSION = "1.48.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mpevk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.10-gatesgarth"
TUNE_FEATURES = "aarch64 armv8a crc cortexa53 crypto"


I am getting below build error:

ERROR: gtk+3-3.24.22-r0 do_package: Error executing a python function in exec_python_func() autogenerated:

The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_python_func() autogenerated', lineno: 2, function: <module>
0001:
*** 0002:sstate_task_postfunc(d)
0003:
File: '/home/shiv/bin/imx-yocto-bsp/sources/poky/meta/classes/sstate.bbclass', lineno: 766, function: sstate_task_postfunc
0762:
0763: omask = os.umask(0o002)
0764: if omask != 0o002:
0765: bb.note("Using umask 0o002 (not %0o) for sstate packaging" % omask)
*** 0766: sstate_package(shared_state, d)
0767: os.umask(omask)
0768:
0769: sstateinst = d.getVar("SSTATE_INSTDIR")
0770: d.setVar('SSTATE_FIXMEDIR', shared_state['fixmedir'])
File: '/home/shiv/bin/imx-yocto-bsp/sources/poky/meta/classes/sstate.bbclass', lineno: 642, function: sstate_package
0638: tmpdir = d.getVar('TMPDIR')
0639:
0640: sstatebuild = d.expand("${WORKDIR}/sstate-build-%s/" % ss['task'])
0641: d.setVar("SSTATE_CURRTASK", ss['task'])
*** 0642: bb.utils.remove(sstatebuild, recurse=True)
0643: bb.utils.mkdirhier(sstatebuild)
0644: for state in ss['dirs']:
0645: if not os.path.exists(state[1]):
0646: continue
File: '/home/shiv/bin/imx-yocto-bsp/sources/poky/bitbake/lib/bb/utils.py', lineno: 685, function: remove
0681: # shutil.rmtree(name) would be ideal but its too slow
0682: cmd = []
0683: if ionice:
0684: cmd = ['ionice', '-c', '3']
*** 0685: subprocess.check_call(cmd + ['rm', '-rf'] + glob.glob(path))
0686: return
0687: for name in glob.glob(path):
0688: try:
0689: os.unlink(name)
File: '/usr/lib/python3.6/subprocess.py', lineno: 311, function: check_call
0307: if retcode:
0308: cmd = kwargs.get("args")
0309: if cmd is None:
0310: cmd = popenargs[0]
*** 0311: raise CalledProcessError(retcode, cmd)
0312: return 0
0313:
0314:
0315:def check_output(*popenargs, timeout=None, **kwargs):
Exception: subprocess.CalledProcessError: Command '['rm', '-rf', '/home/shiv/bin/imx-yocto-bsp/buildmedia/tmp/work/cortexa53-crypto-mx8mp-poky-linux/gtk+3/3.24.22-r0/sstate-build-package/']' died with <Signals.SIGABRT: 6>.

ERROR: Logfile of failure stored in: /home/shiv/bin/imx-yocto-bsp/buildmedia/tmp/work/cortexa53-crypto-mx8mp-poky-linux/gtk+3/3.24.22-r0/temp/log.do_package.6839
ERROR: Task (/home/shiv/bin/imx-yocto-bsp/sources/poky/meta/recipes-gnome/gtk+/gtk+3_3.24.22.bb:do_package) failed with exit code '1'

Can you pls help me solve this??

 

 

0 Kudos
Reply
0 Replies