Build / checksum errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build / checksum errors

3,978 次查看
gfine1
Contributor III

We have a custom i.mx8QM based board. 

Upon the shift from codeaurora to github we are now getting checksum errors when recompiling for u-boot changes. 

We have to modify u-boot to change where we boot from if a GPIO is turned on.  The errors started when codeaurora was sunsetted. 

Is there a simple workaround? 

 

0 项奖励
回复
6 回复数

3,967 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @gfine1, 

NXP continues updating GitHub repositories. It is possible that some branches or components don't work at all, we are working to solve these issues.

Additionally, could you please share more information about the version of Linux or Uboot?

Sorry for any inconvenience this may cause.

Best regards, Brian.

0 项奖励
回复

3,956 次查看
gfine1
Contributor III

We are using an older version (4.14) because our UK development locked down at that version. 

The errors we are running into are checksum errors while recompiling u-boot. I'll have to ask a fellow developer to give me a log of the errors. 

For me a vsftpd recipe attempts a do_patch and fails because it says the "patch was already applied". A day earlier (3/30) it built without a problem. 

 

 

0 项奖励
回复

3,929 次查看
gfine1
Contributor III

It turns out the checksum errors for u-boot were resolved by changing the recipes to point to github.

However, my error still exists. 

WARNING: vsftpd-3.0.3-r0 do_patch: workdir = %s/home/gfine/build-modela/tmp/work/aarch64-poky-linux/vsftpd/3.0.3-r0
WARNING: vsftpd-3.0.3-r0 do_patch: S dir = %s/home/gfine/build-modela/tmp/work/aarch64-poky-linux/vsftpd/3.0.3-r0/vsftpd-3.0.3
WARNING: vsftpd-3.0.3-r0 do_patch: workdir = %s/home/gfine/build-modela/tmp/work/aarch64-poky-linux/vsftpd/3.0.3-r0
WARNING: vsftpd-3.0.3-r0 do_patch: S dir = %s/home/gfine/build-modela/tmp/work/aarch64-poky-linux/vsftpd/3.0.3-r0/vsftpd-3.0.3
ERROR: vsftpd-3.0.3-r0 do_patch: Command Error: 'quilt --quiltrc /home/gfine/build-modela/tmp/work/aarch64-poky-linux/vsftpd/3.0.3-r0/recipe-sysroot-native/etc/quiltrc push' exited with 0 Output:
Patch vsftpd-configuration.patch is already applied; check your series file
ERROR: vsftpd-3.0.3-r0 do_patch: Function failed: patch_do_patch
ERROR: Logfile of failure stored in: /home/gfine/build-modela/tmp/work/aarch64-poky-linux/vsftpd/3.0.3-r0/temp/log.do_patch.5345
ERROR: Task (/home/gfine/sources/meta-openembedded/meta-networking/recipes-daemons/vsftpd/vsftpd_3.0.3.bb:do_patch) failed with exit code '1'

 

0 项奖励
回复

3,906 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @gfine1, 

Thanks for your reply.

It seems the error is for the BSP issues, the internal team continue updating the imx manifest based on GitHub repositories.

Please be patient.

Best regards, Brian.

0 项奖励
回复

3,903 次查看
gfine1
Contributor III

Will do.  I'll wait on a resolution from the BSP team.  Is there any place I can monitor for the fixes? 

Glen

 

0 项奖励
回复

3,883 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @gfine1,

Thank you, I will update you about this case.

Best regards, Brian.

0 项奖励
回复