Build and Pre-build Images are not bootimg in Pico IMX8M Mini Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build and Pre-build Images are not bootimg in Pico IMX8M Mini Board

Jump to solution
1,202 Views
mohamed_gaseen
Contributor IV

Hello,

I'm currently working on Pico I.MX8M  Mini board and I have both the build and pre-built image binaries(below I have attached). Following document will work for technexion pico imx8 m mini board. But whenever I'm flashing with SD CARD flashing mode I'm getting this below errors. I have attached the logs below.

Yocto Build Doc

---------------------

https://www.nxp.com/docs/en/user-guide/RTEDGEYOCTOUG.pdf

Pre-Built Bin Doc

-----------------------

https://www.nxp.com/docs/en/user-guide/REALTIMEEDGEUG.pdf

 

Error Logs

--------------

 

BuildInfo:
- ATF 3c1583b

MMC: no card present
flash target is MMC:1
MMC: no card present
MMC card init failed!
MMC: no card present
** Block device MMC 1 not supported
Net: eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
starting USB...
Bus usb@32e40000: Port not available.
USB is stopped. Please issue 'usb start' first.
MMC: no card present
switch to partitions #0, OK
mmc2(part 0) is current device
Scanning mmc 2:1...
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
MMC: no card present
Scanning disk mmc@30b50000.blk...
Disk mmc@30b50000.blk not ready
Scanning disk mmc@30b60000.blk...
Fou
nd 3 disks
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
Running BSP bootcmd ...
MMC: no card present
MMC: no card present
Couldn't find partition mmc 1:1
Can't set block device
MMC: no card present
Couldn't find partition mmc 1:1
Can't set block device
Booting from net ...
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
BOOTP broadcast 11
BOOTP broadcast 12
BOOTP broadcast 13
BOOTP broadcast 14
BOOTP broadcast 15
BOOTP broadcast 16
BOOTP broadcast 17

Retry time exceeded; starting again
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7

------------------------------------------------------------------------------------------------------------------------------------------------

 

Welcome to minicom 2.7.1

OPTIONS: I18n
Compiled on Dec 23 2019, 02:06:26.
Port /dev/ttyUSB0, 18:35:36

Press CTRL-A Z for help on special keys


U-Boot SPL 2023.04-uboot_v2023.04-2.7.0+g413e0aea79 (Dec 12 2023 - 21:42:36 +0000)
Can't find PMIC:PCA9450
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from MMC1
mmc_load_image_raw_sector: mmc block read error
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

 

Can you please help me to sort out this issue I'm facing.

 

Thanks in Advance.

0 Kudos
Reply
1 Solution
1,184 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @mohamed_gaseen!
Thank you for contacting NXP Support!

Those documents are only for our boards.

Please contact Technexion Support to obtain the correct images for your board.

Best Regards!
Chavira

View solution in original post

0 Kudos
Reply
1 Reply
1,185 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @mohamed_gaseen!
Thank you for contacting NXP Support!

Those documents are only for our boards.

Please contact Technexion Support to obtain the correct images for your board.

Best Regards!
Chavira

0 Kudos
Reply