Build System Derived Toolchain:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build System Derived Toolchain:

2,739 Views
1990rahulreddy
Contributor IV

I have install cross tollchain using SDK, but, when I start ecplise, it showing nothing in "Target Architecture",

also, I am confuse in Toolchain root location & sysroot location.

I have install toolchain in /opt/fsl-imx-x11/3.14.52-1.1.0/

Labels (3)
0 Kudos
Reply
5 Replies

2,427 Views
aravinthkumarja
Senior Contributor II

Hi RahulReddy

Toolchain location --> Cross compiler path

sysroot location --> Filesystem path

You should specify both location properly, Then it will work. I hope it will help full for you.

Regards,

Aravinth

0 Kudos
Reply

2,427 Views
1990rahulreddy
Contributor IV

I am able to get it in "Standalone", but not in "Build System "

0 Kudos
Reply

2,428 Views
aravinthkumarja
Senior Contributor II

Hi RahulReddy

Can you elaborate your issue, Exactly issue i didn't get.

Regards,

Aravinth

0 Kudos
Reply

2,428 Views
1990rahulreddy
Contributor IV

I have created new thread, please give solution..

object detection using haarcascade

0 Kudos
Reply

2,428 Views
gusarambula
NXP TechSupport
NXP TechSupport

I'm just adding the information marked as an answer from the new thread for completeness:

Building OpenCV on ubuntu hardfloat rootfs for i.MX6Q

0 Kudos
Reply