Boundary Scan for MCIMX6Q5EYM12AD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boundary Scan for MCIMX6Q5EYM12AD

1,230件の閲覧回数
bhagathsingh
Contributor I

Hello,

I am trying to run a boundary scan on MCIMX6Q5EYM12AD using J-link from IAR Systems and TopJTAG Probe software tool. Below is the board settings which I have used

TEST_MODE is Low;

JTAG_MOD is High;

POR_B is High;

BOOT_MODE[1:0] is [1:0].

 

When I try to detect the JTAG devices connected, it shows No JTAG Chain Detected. Kindly help me resolve this issue.

Thanks

Bhagath

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,051件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bhagath

one can check jtag signal levels for both processor and JTAG device,

check clocks and power supplies described in i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

[SOLVED] How to do a simple JTAG (boundary) scan? - J-Link/Flasher related - SEGGER - Forum 

Isues with usage TopJTAG Probe software can be posted on support forum for that software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------