Bootloader issues with SABRE iMX6Dl

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader issues with SABRE iMX6Dl

6,102件の閲覧回数
k2
Contributor III

The board doesn't see the bootloader on the SD card. I followed the user guide instructions for setting up a bootable SD card. Is there some code onboard that has to change ? The board came with Android by mistake. It works fine with the Android. Our design is to use the linux. Im using the downloaded bootloader images freescale supplied.

ラベル(2)
タグ(3)
14 返答(返信)

5,571件の閲覧回数
sinanakman
Senior Contributor III

FWIW, I am using the ToT mainline u-boot and flashing with seek=1 bs=1k so I am not sure what that no padding refers to. Let me know if you need more information.

0 件の賞賛
返信

5,571件の閲覧回数
EdSutter
Senior Contributor II

Just a bit more regarding padding...

I spent a few days stumbling on this when using mainline uboot.

Refer to this thread for more info... https://community.freescale.com/thread/315097

Ed

0 件の賞賛
返信

5,571件の閲覧回数
EdSutter
Senior Contributor II

Sinan,

Just curious, what is 'ToT' mainline?

Ed

0 件の賞賛
返信

5,571件の閲覧回数
sinanakman
Senior Contributor III

Hi Ed, sorry for the acronyms. With ToT I refer to tip of the tree for the mainline git trees.

Thanks

Sinan Akman

0 件の賞賛
返信

5,571件の閲覧回数
LeonardoSandova
Specialist I

Correct. seek=1 bs=1k is fine, what I wrote is to omit the 'skip' parameter NOT the seek. More info on

uboot-imx.git - Freescale i.MX u-boot Tree

0 件の賞賛
返信

5,571件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Please send following info: what demo image are you using and exact command line you use to program u-boot to SD card.

And please check Linux User's Guide for info on programming bootloader/kernel/file system from command line in Linux.

0 件の賞賛
返信

5,571件の閲覧回数
k2
Contributor III

Heres what i tried.

We have the iMX6DL SABRE for Smart Devices board with a 10 in LCD.

i'm using the SD3 slot (J507) with SW6 settings of 2 & 7 = ON.

The linux commands i used are :

sudo dd if=u-boot-mx6dl-sabresd.bin of=/dev/sdb seek=2 skip=2 bs=512

the SD card is seen as sdb and sdb1 is the partition.

Kevin

0 件の賞賛
返信

5,571件の閲覧回数
EdSutter
Senior Contributor II

A few thoughts...

1...

You may want to try to add "conv=fsync" to your dd line...

    sudo dd if=u-boot-mx6dl-sabresd.bin of=/dev/sdb seek=2 skip=2 bs=512 conv=fsync

2...

I wasted some time because I had an old (non-high-density) card reader

with a high-density card.  Make sure you're using a relatively new reader (or a low-density SD card).


Ed

0 件の賞賛
返信

5,571件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Agree with this, have seen some older SD card readers cause problems with SDHC cards. Please try with different SD card reader to see if it changes anything.

Other thing to try would be to dump /dev/sdb and make sure that bootloader is written correctly.

0 件の賞賛
返信

5,571件の閲覧回数
sinanakman
Senior Contributor III

Hi Kevin, I have an sabre sd and I am running mainline u-boot without a problem. One thing you might want to keep an eye is, sabre sd will try to boot from the flash first. By holding certain buttons during boot you can force it to boot from SD. But the easiest is to wipe out what you have in the eMMC flash and when it fails to boot from there it will boot from your SD.

Hope this helps

Sinan Akman

0 件の賞賛
返信

5,571件の閲覧回数
LeonardoSandova
Specialist I

Which u-boot version are you using? 2013's u-boots are not padded, so they must be flash without the skip=2 and using the .imx binary. Also, As Ed metioned, make sure you sync.

0 件の賞賛
返信

5,571件の閲覧回数
sinanakman
Senior Contributor III

Hi Leonardo, thanks for the nice summary below. I just realized that what you were asking me above, you were probably intending asking to Kevin. As you confirmed, with seek and without skip I run u-boot without a problem. I only use the mainline u-boot though.

Thanks

Sinan Akman

5,571件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, King

     You mean you are using i.MX6D SabreSD board or SabreAuto board? And it works fine booting up Android, but when you burn bootloader image to a SD card, it still boots up with Android? Please check the boot mode selection, make sure it boots up from the SD slot you want, and also make sure you have a bootable SD card, which means the uboot should write to the right place of SD card. Let me know you boot selection and uboot first, thanks.

0 件の賞賛
返信

5,571件の閲覧回数
k2
Contributor III

We have the iMX6DL SABRE Smart Devices board that comes with the 10 in. LCD. (1000 bucks/board).

It came with a an Android SD card image even thou we ordered LINUX.

So i'm stuck with being able to boot up Android using the Freescale supplied SD.

I followed the User Guide instructions to use the prebuilt images for u-boot and kernel for making a bootable SD card using the linux "dd" commands. Is there any special SW6 settings for booting to LINUX versus the Android ?

I dont see any documentation saying anything. I have (SW6) switches 2 and 7 - ON, rest OFF.

Its apparent that the bootloader isn't running. I'm monitoring the serial debug with minicom.

It works with Android but not with Linux u-boot. I've tried a bunch of different u-boot images. No luck.

So i'm looking for what i missed on this ?

0 件の賞賛
返信