Bootloader MIPI DSI Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader MIPI DSI Driver

3,336 Views
thomasschaefer
Contributor III

Hi all,

we want to enable display support from u-boot bootloader for our i.MX7D based custom board. Our LVDS display is attached to MIPI DSI interface via LVDS bridge.

Unfortunately, current u-boot version does not provide support for the MIPI DSI interface of the i.MX7 CPU. Are there plans or work in progress to add support for i.MX7 MIPI DSI to u-boot?

Is there a linux driver available that could be ported?

Labels (3)
0 Kudos
Reply
2 Replies

2,451 Views
thomasschaefer
Contributor III

Hello Weidong,

not sure if we can use this for i.MX7 as the register interface is quite different compared to i.MX6?

Thank you,

Thomas

0 Kudos
Reply

2,451 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Thomas,

    you can refer to 'the patch for i.MX6 u-boot mipi dsi' to port yours! see the link, please!

Patch to support MIPI display(hx8369) in uboot for i.mx6DL/DQ SebreSD boards 


Have a great day,
TIC Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply