Booting with android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting with android

2,408件の閲覧回数
alexandredel
Contributor I

Hello

I have a Sabrelite with a U-boot made with ltib, I flashed it, then it works perfectly, but i want to put android on it. I'm not sure about the method, i used the android release on a sd card, then i put it in the card. But now, nothing happened. Am i supposed to flash the new u-boot? So why i needed to flash the ltib one?

Best regards

Alexandre

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,259件の閲覧回数
alexandredel
Contributor I

If it can help, i am on ubuntu 10.04

0 件の賞賛
返信

2,259件の閲覧回数
EricNelson
Senior Contributor II

Hello Alexandre,

In general, you shouldn't need to coordinate the U-Boot version doesn't need to match up with the version of Android, since all of our U-Boot's should be configured to launch a boot script named 6x_bootscript from one of the available sources (SD card, SATA, USB memory stick) and our Android images contain a boot script to update the filesystem mounts appropriately.

0 件の賞賛
返信

2,259件の閲覧回数
alexandredel
Contributor I

Hello

So can you tell me where i can find these images and how i put them on the sd card?

Thanks

Alexandre

0 件の賞賛
返信