Booting problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting problem

Jump to solution
5,835 Views
srinivasmuthe
Contributor I

Dear all,

        As I posted  in the discussion

WiFi&BT Related kernel panic in mx53 SMD tablet

the issue causes those kind of problems and It has not booting even when I have just press the Hard reset button or when I just give the command

adb reboot-bootloader in the ADB console.

  In serial down-loader mode also it cannot able to detect by Host.

by these things and as I mentioned previously in

WiFi&BT Related kernel panic in mx53 SMD tablet

the problem  was left by removing Wifi and Bt module, but while autooboot  stop has not worked and while I am opening camera ,It gave error and the serial console at that time is

Unhandled fault: external abort on non-linefetch (0x1018) at 0x4155a054

Unhandled fault: external abort on non-linefetch (0x1018) at 0x414a8054

Unhandled fault: external abort on non-linefetch (0x1018) at 0x414ca054

Unhandled fault: external abort on non-linefetch (0x1018) at 0x414db054

pmem: request for physical address of pmem regimxc_ipu mxc_ipu: Channel already

disabled 10

mxc_ipu mxc_ipu: Channel already uninitialized 10

mxc_ipu mxc_ipu: Channel already disabled 10

mxc_ipu mxc_ipu: Channel already uninitialized 10

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

mxc_v4l_close: release resource



So, Kindly suggest me regarding the issue....please.


thanks&regards,

Muthe.




0 Kudos
Reply
1 Solution
4,412 Views
lily_zhang
NXP Employee
NXP Employee

Hello, Muthe:

From above descriptions, do you have chance to check relative power supplies are still normal in your board?

For such kind of logs, it's normal if the use cases use FSL audio codec:

Unhandled fault: external abort on non-linefetch (0x1018) at 0x4155a054


View solution in original post

0 Kudos
Reply
5 Replies
4,413 Views
lily_zhang
NXP Employee
NXP Employee

Hello, Muthe:

From above descriptions, do you have chance to check relative power supplies are still normal in your board?

For such kind of logs, it's normal if the use cases use FSL audio codec:

Unhandled fault: external abort on non-linefetch (0x1018) at 0x4155a054


0 Kudos
Reply
4,412 Views
srinivasmuthe
Contributor I

hello Xiaoli Zhang,

    Thanks for you support ,

          The boot ROM code has to intialize the UART And in Serial Download mode it has to communicate with Host.

These two cases have failed , Is that due to damage of any Hardware or processor,

thanks&regards,

Muthe.

0 Kudos
Reply
4,412 Views
lily_zhang
NXP Employee
NXP Employee

Hello, Muthe:

I am not sure. Do you have asked any Hardware guy to check your board? We didn't meet such kind of problems in our side. If no HWguy helps to check your board yet, i will check with our HW engineer and see whether he can give some advices.

4,412 Views
srinivasmuthe
Contributor I

Hello, Xiaoli Zhang ,

I did not discuss this problem with any freescale HW guy &,Could you please help me regarding that with your HW guys ..

Thank you for your continuous support.

Thanks&regards,

Muthe.

0 Kudos
Reply
4,412 Views
srinivasmuthe
Contributor I

Hi..

The board voltages at PMIC has some problems such as the VLDO8_1V8(voltage across c213) ,It is showing short circuit with 3.3 voltage i.e VLDO3_3V3(voltage across c194).

  Can you Help me regard this Hardware malfunctioning of my board.

thanks&regards,

Muthe.

0 Kudos
Reply