Booting linux from NAND Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting linux from NAND Flash

3,233件の閲覧回数
cnguyenterasci
Contributor I

When I boot my device from NAND flash, everything goes ok but it just stops booting at "Waiting for root device /dev/mmcblk0p3..."

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

2,900件の閲覧回数
cnguyenterasci
Contributor I

I ran the MFG Tool and loaded linux on the NAND flash.  I h ave the jumpers set to be booting from NAND flash as well. 

0 件の賞賛
返信

2,899件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

When the board booting up, there is a "Kernel Command line". Please check the root filesystem location. it should be something like "root=/dev/xxxxxxxx". For NAND, should be like this root=/dev/mtdblock1.

2,899件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Is your filesystem store in the SD Card? according to your message, it is looking for the rootfs from the SD Card (mmcblk0) partition 3. Please double check the bootargs in uboot used is correct or not.

0 件の賞賛
返信

2,899件の閲覧回数
sinanakman
Senior Contributor III

Calvin, which device, which board is this ?

0 件の賞賛
返信

2,899件の閲覧回数
cnguyenterasci
Contributor I

i.Mx233.  I have an EVK board as well as a board I designed and I get the same thing on both boards.

0 件の賞賛
返信