Booting Dual plus Q7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting Dual plus Q7

1,555 次查看
manjunathjoshi
Contributor V

Hello All,

I have a working bootloader 2015.04 for quad plus i.mx6 SOM. But when i use the same bootloader for dual plus,

1. It doesn't boot

or

2. It might be booting but i don't see anything on console.

I was wondering what could be the issue?

Is there any major difference that would cause an issue in booting dual plus?

Regards,

Manju

标签 (2)
0 项奖励
回复
2 回复数

1,450 次查看
RossMcLuckie
NXP Employee
NXP Employee

Hi,

There should be no difference when booting Dual versus Quad, you should check your SOM module for issues, if you have only tested one board it would seem more likely to be a board/build issue than a silicon one.

Regards

Ross

0 项奖励
回复

1,450 次查看
RossMcLuckie
NXP Employee
NXP Employee

PS if you have not already seen the Hardware Developers Guide, you should take a look at that, it has some helpful information for bringing boards up and checking for issues -

i.MX6QP|i.MX 6QuadPlus Processors|Quad Core|NXP 

Click on the User Guides filter on the left.

Regards

Ross

0 项奖励
回复