Booting Dual plus Q7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting Dual plus Q7

1,597 Views
manjunathjoshi
Contributor V

Hello All,

I have a working bootloader 2015.04 for quad plus i.mx6 SOM. But when i use the same bootloader for dual plus,

1. It doesn't boot

or

2. It might be booting but i don't see anything on console.

I was wondering what could be the issue?

Is there any major difference that would cause an issue in booting dual plus?

Regards,

Manju

Labels (2)
0 Kudos
Reply
2 Replies

1,492 Views
RossMcLuckie
NXP Employee
NXP Employee

Hi,

There should be no difference when booting Dual versus Quad, you should check your SOM module for issues, if you have only tested one board it would seem more likely to be a board/build issue than a silicon one.

Regards

Ross

0 Kudos
Reply

1,492 Views
RossMcLuckie
NXP Employee
NXP Employee

PS if you have not already seen the Hardware Developers Guide, you should take a look at that, it has some helpful information for bringing boards up and checking for issues -

i.MX6QP|i.MX 6QuadPlus Processors|Quad Core|NXP 

Click on the User Guides filter on the left.

Regards

Ross

0 Kudos
Reply