Booting Dual plus Q7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting Dual plus Q7

1,549件の閲覧回数
manjunathjoshi
Contributor V

Hello All,

I have a working bootloader 2015.04 for quad plus i.mx6 SOM. But when i use the same bootloader for dual plus,

1. It doesn't boot

or

2. It might be booting but i don't see anything on console.

I was wondering what could be the issue?

Is there any major difference that would cause an issue in booting dual plus?

Regards,

Manju

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,444件の閲覧回数
RossMcLuckie
NXP Employee
NXP Employee

Hi,

There should be no difference when booting Dual versus Quad, you should check your SOM module for issues, if you have only tested one board it would seem more likely to be a board/build issue than a silicon one.

Regards

Ross

0 件の賞賛
返信

1,444件の閲覧回数
RossMcLuckie
NXP Employee
NXP Employee

PS if you have not already seen the Hardware Developers Guide, you should take a look at that, it has some helpful information for bringing boards up and checking for issues -

i.MX6QP|i.MX 6QuadPlus Processors|Quad Core|NXP 

Click on the User Guides filter on the left.

Regards

Ross

0 件の賞賛
返信