Booting Android on SabreSD hangs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting Android on SabreSD hangs

1,091 次查看
poonguzhalip
Contributor II

When I have the file system mounting in a separate fstab.freescale file and mount the file system with the below line in the init.rc file

on fs

      mount_all /fstab.freescale

with the contents of fstab.freescale as below

/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc1 /mnt/media_rw/extsd vfat defaults voldmanaged=extsd:auto

/devices/platform/fsl-ehci /mnt/media_rw/udisk vfat defaults voldmanaged=udisk:auto

/dev/block/mmcblk0p5    /system      ext4    ro                                                                               wait

everything works fine. i.e I am able to boot the device successfully.

But when I try to mount the partitions directly instead of using a fstab.freescale file like below

on fs

# mount ext4 partitions

#    mount_all /fstab.freescale

    mount vfat /devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc1 /mnt/media_rw/extsd defaults

    mount vfat /devices/platform/fsl-ehci /mnt/media_rw/udisk defaults

    mount ext4 /dev/block/mmcblk0p5 /system ro remount

then while booting, it hangs after  "Freeing init memory: 248K".

I am using Android 4.4 on SabreSD board.

Any ideas on how I can solve this?

Regards

0 项奖励
回复
0 回复数