Boot2QT for i.mx8 mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot2QT for i.mx8 mini

ソリューションへジャンプ
4,472件の閲覧回数
jdluhy
Contributor II

Has anyone done a boot2qt image for the i.mx8 mini nxp board. I have built the qt xwayland yocto image and not sure how to create a toolchain and boot2qt image for commercial QT with support for this board. The board is 8MMINILPD4-EVK. 

ラベル(1)
0 件の賞賛
返信
1 解決策
4,328件の閲覧回数
jdluhy
Contributor II

I was able to create a boot2qt qbsp for the imx8mmevk. For others looking at this, it really did not require much to do. Only changed one line in a .conf file and created a file imx8mmevk.conf to match the others. Was able to boot into qt and run samples. Was also able to debug through usb.

元の投稿で解決策を見る

4 返答(返信)
4,328件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello James Dluhy,

It is my understanding that Boot2Qt changed its name to Qt for Device Creation. There is no support for the i.MX8M Mini that I’m aware (I may be wrong, as it’s supported directly by Qt), but there is support for some i.MX8 boards.

https://doc.qt.io/QtForDeviceCreation/qtee-preparing-hardware-nxp-imx-8quad.html

I would recommend contacting Qt or looking for more information on Qt centric forums.

My apologies for the inconvenience.

Regards,

0 件の賞賛
返信
4,328件の閲覧回数
jdluhy
Contributor II

Thanks,

    I have been in touch with QT. They wanted $10K to create a boot2qt

so I have been looking at trying to build it. I have been folowing

another board branch of meta-boot2qt that I should be able to follow. - Jim

0 件の賞賛
返信
4,329件の閲覧回数
jdluhy
Contributor II

I was able to create a boot2qt qbsp for the imx8mmevk. For others looking at this, it really did not require much to do. Only changed one line in a .conf file and created a file imx8mmevk.conf to match the others. Was able to boot into qt and run samples. Was also able to debug through usb.

4,328件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello James Dluhy, 

Thank you for updating this thread. I'm sure it will help other Community Users looking to implement boot2qt.

Regards,

0 件の賞賛
返信