Boot without external RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot without external RTC

ソリューションへジャンプ
3,043件の閲覧回数
AdrianMerrath
Contributor III

Hello,

we designed our own i.MX 8M Hardware and it is not possible to boot without an external 32kHz clock. When we connect a external 32kHz clock there are no Bootproblems.

The Datasheet says: "When an external RTC clock input is not present, the 32 kHz clock for internal logic is generated by the 25 MHz oscillator".

Is this a known issue?

Thanks in advance.

Best regards,

Adrian

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,782件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   External RTC clock is mandatory.

All three clock sources (RTC clock,  XTAL 25M, XTAL 27M) are mentioned explicitly

as must be running in the i.MX8M Hardware Developer’s Guide.

  The Datasheet(s) should be updated in order to remove the following statement:

"When an external RTC clock input is not present, the 32 kHz clock for internal logic

is generated by the 25 MHz oscillator".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,783件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   External RTC clock is mandatory.

All three clock sources (RTC clock,  XTAL 25M, XTAL 27M) are mentioned explicitly

as must be running in the i.MX8M Hardware Developer’s Guide.

  The Datasheet(s) should be updated in order to remove the following statement:

"When an external RTC clock input is not present, the 32 kHz clock for internal logic

is generated by the 25 MHz oscillator".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,782件の閲覧回数
AdrianMerrath
Contributor III

Hello Yuri,

thank you very much for your help. This is an important information for our redesign.

Best regards,

Adrian

0 件の賞賛
返信