Hi all
My customer would like to reset the system using the WDT timeout reset.
However, they can't success.
In this situation, we have some questions about boot sequence of i.MX7D.
Q1
They don't input to POR at the time of WDT reset.
Do they have to input POR ?
Q2.
According to the Figure 6-20 in IMX7DRM, there are some branch.
What is the criteria of "Check Reset Type" branch ?
In other word, what do you mean the "Normal" ?
Q3
In the "Download Initial boot Image(primary or secondary depending on persistent bit)" branch, what is the criteria ?
My understanding is only checking a vector table and persistent bit. Am I correct ?
Ko-hey
Solved! Go to Solution.
 joanxie
		
			joanxie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		1) refer to the RM:"During reset, the chip checks Power Gating Controller status register." so for the detailed status, pls refer to the PGC, refer to the flow, besides of nomally mode, another is waking up from low power boot mode
2) yes
 joanxie
		
			joanxie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		1) refer to the RM:"During reset, the chip checks Power Gating Controller status register." so for the detailed status, pls refer to the PGC, refer to the flow, besides of nomally mode, another is waking up from low power boot mode
2) yes
 
					
				
		
Hi joanxie
Thank you for reply.
Let me confirm your answer.
Q4
"Check Reset Type" branch checks the Power Gating Controller status register.
So when user want to waking up from low power boot mode, it will goes to "Is Wakeup allowed" branch.
Am I correct ?
Do you have any example of PGC register when user do WDT reset ?
Q5
The answer of 2) is for Q3. Am I correct ?
Ko-hey
 joanxie
		
			joanxie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		yes, right for two questions, sorry, we don't have such example for this.