Boot mode Imx8mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot mode Imx8mini

2,101件の閲覧回数
idom
Contributor II

Hi 

I custome board with IMX8mini.

I have two issues:

1. When boot mode0=0 and boot_mode1=0 the boot sequence does not start,

2. When Boot_mode0=1 or 0 and Boot_mode1=1  boot seqeunce start and finished but only when the UART-USB DBG connected to the terminal.

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,980件の閲覧回数
idom
Contributor II

Hello Igor

With my custom board I have flashed with UUU the original NXP's Android kernel (the NXP default U boot) port(without making any changes to it). So, I suppose that BT_FUSE_SEL should be already programmed similar to the NXP EVM ?

0 件の賞賛
返信

1,980件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ido

boot mode0=0 and boot_mode1=0 selects boot from fuses, which probably not programmed.

For details one can look at sect.6.1.2.3 Boot From Fuses mode (BOOT_MODE[1:0] = 00b)

i.MX 8M Mini Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信