Boot issue in imx6Q sabre-AI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot issue in imx6Q sabre-AI

2,706 次查看
suhaskaundinya
Contributor I

Hello guys,

I am using i.MX 6Quad SABRE-AI with Andriod N.

I tried to flash the images on the sdcard using

$ sudo chmod +x ./device/fsl/common/tools/fsl-sdcard-partition.sh
$ sudo ./device/fsl/common/tools/fsl-sdcard-partition.sh -f imx6q /dev/sdc

(Find the above commands in the pdf)

In the prompt, it showed flashing the images onto sd card and it was complete, but when I tried to boot the board using SDcard, I get the following error:

In:    serial                                           
Out:   serial                                           
Err:   serial                                           
Net:   FEC [PRIME]                      
Hit any key to stop autoboot:  0        
switch to partitions #0, OK             
mmc0 is current device                  
** Unrecognized filesystem type **      
** Unrecognized filesystem type **      
Booting from net ...                    
FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !
Could not initialize PHY FEC
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3                                                               
BOOTP broadcast 4                                                               
BOOTP broadcast 5                                                               
BOOTP broadcast 6                                                               
BOOTP broadcast 7                                                               
BOOTP broadcast 8                                                               
BOOTP broadcast 9                                                               
BOOTP broadcast 10                                                              
BOOTP broadcast 11                                                              
BOOTP broadcast 12                                                              
BOOTP broadcast 13                                                              
BOOTP broadcast 14

Could anyone advice me on this?

I have attached the pdf of the document I am referring to, to build Android N on the SD card.

Thanks in advance.

BR,

Suhas

标签 (4)
0 项奖励
回复
3 回复数

2,534 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Suhas

nxp has tool for programming images - mfg tool, please try it,

use mfgtool2-android-mx6q-sabreauto-sdcard.vbs script.

https://www.nxp.com/webapp/Download?colCode=IMX_N7.1.2_2.0.0_TOOL&appType=license&location=null 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,534 次查看
suhaskaundinya
Contributor I

Hello Igor,


Thanks for the tip.

Isn't MFG tool for Windows?

I am using Linux Ubuntu 16.04 LTS.

Is there any other tool wherein I can flash the images? I used dd utility and faced the above issue.

BR,

Suhas

0 项奖励
回复

2,534 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Suhas

please check mfg tool documentation (mfgtoolcli)

https://community.nxp.com/message/893898?commentID=893898#comment-893898 

Best regards
igor

0 项奖励
回复