Boot from usb disk hardware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot from usb disk hardware

ソリューションへジャンプ
1,040件の閲覧回数
zh_y
Contributor II

My board platform is i.MX6QP .I want to start uboot, kernel and rootfs from usb disk hardware. Is there any good way?

0 件の賞賛
返信
1 解決策
916件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Unfortunately,

That is impossible, the only boot devices for the i.MX6Q are the following ones:

• NOR flash
• NAND flash
• OneNAND flash
• SD/MMC
• Serial ATA (SATA) HDD (only i.MX 6Dual/6Quad)
• Serial (I2C/SPI) NOR flash and EEPROM

Best regards,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
917件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Unfortunately,

That is impossible, the only boot devices for the i.MX6Q are the following ones:

• NOR flash
• NAND flash
• OneNAND flash
• SD/MMC
• Serial ATA (SATA) HDD (only i.MX 6Dual/6Quad)
• Serial (I2C/SPI) NOR flash and EEPROM

Best regards,

Diego.

0 件の賞賛
返信