Boot from Serial flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot from Serial flash

1,333件の閲覧回数
asou_junichi
Contributor I

Hi,

If i.MX6 is accidentally restarted during accessing to the serial flash at upper 128Mb segment with 4-byte addressing mode.

Then i.MX6 tries to reboot from the serial flash with 3-byte addressing mode but the serial flash still stays in 4-byte addressing mode. 

In this case, the serial flash can not be read correctly because there are mismatch of addressing mode between i.MX6 and serial flash.

To avoid this kind of issue, dose the serial flash with hardware reset pin have to be introduced, and resetting the serial flash when i.MX6 is rebooting?

Or are there any other idea?

BR,

JA

ラベル(1)
0 件の賞賛
返信
1 返信

1,281件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 麻生 淳一 

>dose the serial flash with hardware reset pin have to be introduced, and resetting

>the serial flash when i.MX6 is rebooting?

yes this is correct idea.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信