Boot from SPI-NOR flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot from SPI-NOR flash

ソリューションへジャンプ
5,655件の閲覧回数
carmilili
Contributor III

The CPU of my board is i.mx6q.I want to use SPI-NOR flash(32M) to store u-boot kernel and file system.

Now,I have a problem with kernel booting.The u-boot boot up successfully.

Please look at below detail carefully.

The flash has two partition.

/dev/mtd0 4.5M

/dev/mtd1 27.5M

I use MfgTool to burn image and file system.

uxl2:

<CMD state="Updater" type="push" body="$ flash_erase /dev/mtd0 0 0">Erasing Boot partition</CMD>
<CMD state="Updater" type="push" body="send" file="files/u-boot.bin">Sending U-Boot</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mtd0 bs=512">write U-Boot to SPI-NOR</CMD>
<CMD state="Updater" type="push" body="send" file="files/uImage">Sending Kernel Image</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mtd0 bs=512 seek=1000">Flashing Kernel</CMD>

u-boot command

setenv bootargs_sf 'setenv bootargs ${bootargs} ip=${ipaddr} root=/dev/mtdblock1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'

setenv bootcmd_sf 'run bootargs_base bootargs_sf;sf probe 2:0;sf read ${loadaddr} 0x80000 0x400000;bootm'

I think my u-boot image is stored in the first 512k and the kernel image follow the u-boot image.

//-----512k----/------4M-----/---------27.5M-------------//

     u-boot         kernel         file system

//            mtd0             /      mtd1                 //

But now when the u-boot run to end and copy the uImage from flash.It is interrupted by error.

MX6Q SABRESD U-Boot > boot

Wrong Image Format for bootm command

ERROR: can't get kernel image!

My question:

1,Does someone know why it can not find the kernel image?I think the address of kernel image is from 512k to 4.5M.

2,Dose the uImage different from using by MMC and SPI-NOR flash?

ラベル(7)
0 件の賞賛
返信
1 解決策
2,712件の閲覧回数
carmilili
Contributor III

Ha ha,

I solve it.


<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mtd0 bs=512 seek=1000">Flashing Kernel</CMD>

to

<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mtd0 bs=512 seek=1024">Flashing Kernel</CMD>

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,713件の閲覧回数
carmilili
Contributor III

Ha ha,

I solve it.


<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mtd0 bs=512 seek=1000">Flashing Kernel</CMD>

to

<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mtd0 bs=512 seek=1024">Flashing Kernel</CMD>

0 件の賞賛
返信