Boot from SATA ISSUES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot from SATA ISSUES

2,494件の閲覧回数
Chicago1984
Contributor II

I was able to blow the fuse and see that the boot device is now SATA, but now I’m getting a “Card

did not respond to voltage select!” and “MMC init failed” error.  I wonder if there is something in

the code that is still wanting to grab code from the SD card.

Is there an easy way to blow the fuse in the Manufacturing Tool?  I tried to set it up, but being new

to it I was getting no ware slowly.

Image attached.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,241件の閲覧回数
tonyzheng
NXP Employee
NXP Employee

Hello,

It seems that you board is not the official reference board powered by Freescale.

Can you tell me where your kernel and rootfs, in SATA or SD card?

As with SadreSD board, booting from the SATA is supported through changing u-boot configs.

0 件の賞賛
返信

2,241件の閲覧回数
tonyzheng
NXP Employee
NXP Employee

If your kernel and rootfs reside in the SATA SSD, you don't need to detect SD Card.

For more information, you can refer to:

https://community.freescale.com/message/318957#318957

0 件の賞賛
返信