Boot error after WDT reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot error after WDT reset

2,310件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Let me confirm about boot up.

There are following description in P1135 in reference manual.

After reset, the Boot ROM code determines that BT_FUSE_SEL
is blown (BT_FUSE_SEL = 1) and the ROM code performs internal boot according to the new eFUSE settings.

According to the description, after the reset since it is assumed that BT_FUSE_SEL = 1.

I know it follows OTP setting after WDT reset.

However, on the custom board, it goes to the serial downloader mode when trying WDT reset.

What should I check for it ?

Does the word "reset" in the description include WDT reset ?

Ko-hey

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,191件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Looks like internal boot with fuse configuration crashed, therefore internal serial

downloader starts. You may create request to get boot utility to review boot log.

Support|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,191件の閲覧回数
ko-hey
Senior Contributor II

Hi

Is the description in P1135 correct ?

I made the Case 00119672.

Could you follow the case ?

Ko-hey

0 件の賞賛
返信

2,191件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hi,

 

   the description is correct.

I picked up Case 00119672.

Regards,

Yuri.

0 件の賞賛
返信