Boot difference?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot difference?

2,091 Views
marknordstrand
Contributor III

Just got a imx6-sdp board and booted it up.  I had been working with the -sdb board and noticed the new one's u-boot environment was a bit different.  My BSP/u-boot experience isn't that great, and would like to know if there's a good run down on the differences.  I noticed the use of a booti command which I've never seen before.  I imagine this is specific to how the image is set up.  Is my thinking correct? 

Labels (1)
0 Kudos
Reply
2 Replies

1,888 Views
YixingKong
Senior Contributor IV

Mark, has your question been answeed? If yes, please click Correct Answer/Helpful Answer.

Thanks,

Yixing

0 Kudos
Reply

1,888 Views
kmoran
Contributor I

The booti command is used to load and run an Android boot.img file from a memory partition, typically mmc2 or mmc3, etc.

0 Kudos
Reply