Boot custom board from NAND flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot custom board from NAND flash

2,169 次查看
maheshkumarkoda
Contributor III

Hello Community, Hello igorpadykov

1). Could you please let me know from which U-boot version & branch you took these attached files referred in below link?

Nand boot with u-boot 2013.04 on i.mx6 SOLO

Or,

could you attach imximage.cfg file also?

2). Can i directly integrate these files in U-boot version v2015.04+gitAUTOINC+5d9ffd2214-r0 in order to boot from NAND?

3). Does this nand configworks as nand driver to copy U-boot/(next stage bootloader) to NAND flash(i think which initializes iomux and clocks alone)

or

do we need mtd/nand driver from kernel?

NOTE: i don't want to call kernel image in next level, instead i want to load another BL.

Please put some light :smileyhappy:

Thanks,

Mahesh.

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,900 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

it is from

uboot-imx.git - Freescale i.MX u-boot Tree

one can try to integrate to other versions, however I believe it is already integrated to uboot-imx

http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2015.04_4.1.15_1.0.0_ga

Note there may be differencies between uboot-imx (nxp uboot) and u-boot-fslc (community uboot),

general discussion about differencies can be found in

difference between Yocto Community BSP and Freescale BSP Release

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,900 次查看
maheshkumarkoda
Contributor III

Hi Igor,

Thanks for the source link.

Is uboot-imx (nxp uboot) a static - freescale official release BSP?

can I use this source as a reference to build image with cross toolchain locally, without yocto project?

Thanks,

Mahesh.

0 项奖励
回复