Hi everyone,
I'm trying to use HAB for the kernel verification. I managed to sign the kernel image and to get "No HAB Events Found!" calling hab_auth_img 0x40480000 0x13c6f60 0x13c6000.
I have two questions:
Thanks
Paolo Gentili
Hi, just a quick update.
I found a workaround: I modified the booti.c file so that the booti command requires also the image size and the image offset. This way useful also because I need to verify not only the kernel but also the DTB: a modification to booti.c was needed nevertheless.
Thanks
Paolo
Hi,
Thanks for your reply but you misunderstood me, let me explain again.
The kernel is the same, these are the steps to reproduce:
1) Manually load kernel Image at addr x
2) Run hab_auth_img with the kernel size/offset that I know because I compiled it
3) It returns no events, good.
4) Run booti
5) It automatically run an hab_authentication but if fails... (I found out that is related to a wrong kernel size).
So why with the same Image I'm having this problem?
Thanks
Paolo
Hi again,
Thanks for your reply.
I later found out that uboot itself, in the booti routine, tries to verify the kernel.
I have a problem though: the verification run manually by me is fine (via hab_auth_img) but the one performed by uboot fails. I found out that the problem is in the kernel size: my image has size 0x13c6f60 but the size retrieved inside booti_setup is 0x143b020.
Do you know why this is happening?
Thanks
Paolo Gentili