Boot SSD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,552件の閲覧回数
niklasmolin
Senior Contributor I

Hi.

I have just received a Sabre Lite board and trying to boot from the SSD drive (SATA connection).

I managed to mount the SSD drive when running a LTIB image, when booting up from the SD card (use the image provided from (http://boundarydevices.com/ltib-4-0-0-images/).

Then I formatted the SSD in ext3 format (in Ubunut).

mkfs.ext3 -L ltib /dev/sdb

after that I mounted the disk and got /media/ltib

Then I unpacked the LTIB image into the SSD drive:

sudo tar zxvf ltib4-no-x-20130618.tar -C /media/ltib/

But when I boot up my SABRE Lite card (without the SD card) it seems like it is trying to boot from the SSD, but I get following messages:

SATA Device Info:

S/N: FF180738082600047077

Product model number: BP4 mSATA SSD

Firmware version: S8FM06.1

Capacity: 62533296 sectors

SATA device 0: Model: BP4 mSATA SSD Firm: S8FM06.1 Ser#: FF180738082600047077

            Type: Hard Disk

            Supports 48-bit addressing

            Capacity: 30533.8 MB = 29.8 GB (62533296 x 512)

... is now current device

** No partition table - sata 0 **

** No partition table - sata 0 **

It seem like it doesn't like the partitioning on the SSD.

Do I need to create the bootable image on the SSD drive in a different way?

Thanks,

Niklas

タグ(3)
0 件の賞賛
返信
1 解決策
2,242件の閲覧回数
niklasmolin
Senior Contributor I

I found the problem.

I didn't do a sfdisk to create partitioning when I formatted the SSD drive.

Now I can boot direct from the SSD drive.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,243件の閲覧回数
niklasmolin
Senior Contributor I

I found the problem.

I didn't do a sfdisk to create partitioning when I formatted the SSD drive.

Now I can boot direct from the SSD drive.

0 件の賞賛
返信