Boot ROM code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot ROM code

2,008 Views
eishishibusawa
Contributor III

Dear Sir

 

I would like to confirm the boot ROM code of i.MX6Dual.

The customer system boots from the parallel NOR (with Linux).

Q1.

What does it execute with Boot ROM code?

Is there any document that explained it?

 

Best Regards,

Eishi SHIBUSAWA

Labels (2)
0 Kudos
Reply
1 Reply

1,872 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

it is explained in sect.8.5.1.1 NOR flash boot operation i.MX6DQ Reference Manual:


Booting from the NOR flash is supported via the EIM interface. The ROM reads the
Image Vector Table and Boot Data structures to determine if the image can be executed
directly from the EIM address space or copied to another memory.

https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply