Boot ROM code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot ROM code

2,002件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I would like to confirm the boot ROM code of i.MX6Dual.

The customer system boots from the parallel NOR (with Linux).

Q1.

What does it execute with Boot ROM code?

Is there any document that explained it?

 

Best Regards,

Eishi SHIBUSAWA

ラベル(2)
0 件の賞賛
返信
1 返信

1,866件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

it is explained in sect.8.5.1.1 NOR flash boot operation i.MX6DQ Reference Manual:


Booting from the NOR flash is supported via the EIM interface. The ROM reads the
Image Vector Table and Boot Data structures to determine if the image can be executed
directly from the EIM address space or copied to another memory.

https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信